eSM_ClientGetProfileCommand
teZCL_Status eSM_ClientGetProfileCommand(
uint8 u8SourceEndpoint,
uint8 u8DestinationEndpoint,
tsZCL_Address *psDestinationAddress,
uint8 u8IntervalChannel,
uint32 u32EndTime,
uint8 u8NumberOfPeriods);
Description
This function can be used on a Simple Metering cluster client (with the ‘Get Profile’ feature enabled) to send a ‘Get Profile’ request to the Simple Metering cluster server in order to retrieve historical consumption data.
The server contains a circular buffer which stores a sequence of data entries containing consumption data for consecutive time intervals, identified by their end-times. This function can request a number of entries from the buffer, containing the consumption data over multiple intervals.
The function parameters include:
The number of buffer entries (corresponding to consumption intervals) requested
The most recent end-time for which a buffer entry will be reported - the most recent consumption data will be reported which has an end-time equal to or earlier than this end-time (a specified end-time of zero will result in the most recent consumption data)
A value indicating whether the units delivered or units received are being requested
This is a non-blocking function and so returns immediately after the request has been sent. The application must then wait for a response, which is accessed using the function u32SM_GetReceivedProfileData().
Parameters
u8SourceEndpoint: Number of local endpoint through which request is sent
u8DestinationEndpoint: Number of endpoint to which request is sent on the destination device
psDestinationAddress: : Pointer to a structure containing the address of the destination device
u8IntervalChannel: Required consumption data - received or delivered:
E_CLD_SM_CONSUMPTION_RECEIVED
E_CLD_SM_CONSUMPTION_DELIVERED
u32EndTime: A UTC time representing the most recent interval end-time for which data will be reported (a zero value means report data for the most recent interval)
u8NumberOfPeriods: Number of consumption intervals to be reported
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_ZTRANSMIT_FAIL
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_CLUSTER_ID_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_EP_RANGE
Parent topic:Functions