eSM_ServerUpdateConsumption
teZCL_Status eSM_ServerUpdateConsumption(
uint8 u8SourceEndPointId,
uint32 u32UtcTime);
Description
This function can be used on a Simple Metering cluster server (with the ‘Get Profile’ feature enabled) to add a new entry to the circular buffer used to store historical consumption data. The buffer stores a sequence of entries containing consumption data for consecutive time intervals, identified by their end-times.
Before this function is called, the application must update one or both of the following Simple Metering cluster attributes with the relevant consumption(s) over the last time interval (since the last readings were made):
u24CurrentPartialProfileIntervalValueDelivered
u24CurrentPartialProfileIntervalValueReceived
An attribute only needs to be updated if the corresponding consumption has been implemented.
The function takes the current time (UTC time) as an input and adds a buffer entry containing the consumption measurements together with the supplied UTC time, which is saved as the end-time of the interval
The entry is stored as a tsSEGetProfile structure, described in Section 42.11.5.
The buffer can contain a limited number of entries, determined at compile-time (see Section 42.12), and operates on a FIFO basis so that a new entry added to a full buffer will over-write the oldest entry.
The function should be called periodically by the application. The period must match the value to which the Simple Metering eProfileIntervalPeriod attribute has been set (see Section 42.2). Standard periods, ranging from 2.5 minutes to one day, are provided as a set of enumerations (see Section 42.10.10).
Parameters
u8SourceEndPointId: Number of local endpoint on which the Simple Metering cluster server operates
u32UtcTime: Current time (as UTC time which can be obtained using u32ZCL_GetUTCTime())
Returns
E_ZCL_SUCCESS
Parent topic:Functions