Compile-time Options

To enable the Temperature Measurement cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:

#define CLD_TEMPERATURE_MEASUREMENT

In addition, to include the software for a cluster client or server, it is necessary to add one of the following to the same file:

#define TEMPERATURE_MEASUREMENT_CLIENT
#define TEMPERATURE_MEASUREMENT_SERVER

Optional Attribute

Add this line to enable the optional Tolerance attribute:

#define CLD_TEMPMEAS_ATTR_TOLERANCE

Global Attributes

Add this line to enable the optional Attribute Reporting Status attribute:

#define CLD_TEMPMEAS_ATTR_ID_ATTRIBUTE_REPORTING_STATUS

Add this line to define the value (n) of the Cluster Revision attribute:

#define CLD_TEMPMEAS_CLUSTER_REVISION <n>

The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).

Parent topic:Temperature Measurement Cluster