bZCL_GetTimeHasBeenSynchronised

bool_t bZCL_GetTimeHasBeenSynchronised(void);

Description

This function queries whether the ZCL time on the device has been synchronized.

The clock is considered to be unsynchronized at start-up and is synchronized following a call to vZCL_SetUTCtime(). The ZCL time must be synchronized before using the time-related functions of other clusters.

Parameters

  • None

Returns

  • TRUE if the local ZCL time has been synchronized, otherwise FALSE

Parent topic:Functions