Appliances
The Appliances clusters implemented by NXP are listed and outlined in the table below. These clusters are detailed in ‘Part XI: Appliances Clusters’ of this manual.
Cluster |
Cluster ID |
Description |
|---|---|---|
Appliance Control |
0x001B |
The Appliance Control cluster provides an interface for remotely controlling appliances in the home. This cluster is detailed in Chapter 45. |
Appliance Identification |
0x0B00 |
The Appliance Identification cluster provides an interface for obtaining and setting basic appliance information. This cluster is detailed in Chapter 46. |
Appliance Events and Alerts |
0x0B02 |
The Appliance Events and Alerts cluster provides an interface for the notification of significant events and alert situations. This cluster is detailed in Chapter 47. |
Appliance Statistics |
0x0B03 |
The Appliance Statistics cluster provides an interface for supplying statistical information about an appliance. This cluster is detailed in Chapter 48. |
Parent topic:ZCL Member Clusters