Commissioning
The Commissioning clusters implemented by NXP are listed and outlined in the table below. These clusters are detailed in ‘Part X: Commissioning Clusters’ of this manual.
Cluster |
Cluster ID |
Description |
|---|---|---|
Commissioning |
0x0015 |
The Commissioning cluster can be used for commissioning the ZigBee stack on a device during network installation and defining the device behaviour with respect to the ZigBee network (it does not affect applications operating on the devices). This cluster is detailed in Chapter 43. |
Touchlink Commissioning |
0x1000 |
The Touchlink Commissioning cluster is used when forming a ZigBee 3.0 network or adding a new node to an existing network. This cluster is detailed in Chapter 44. |
Parent topic:ZCL Member Clusters