Lighting
The Lighting clusters implemented by NXP are listed and outlined in the table below. These clusters are detailed in ‘Part V: Lighting Clusters’ of this manual.
Cluster |
Cluster ID |
Description |
|---|---|---|
Colour Control |
0x0300 |
The Colour Control cluster can be used to adjust the colour of a light (it does not govern the overall luminance of the light, as this is controlled using the Level Control cluster). This cluster is detailed in Chapter 31. |
Ballast Configuration |
0x0301 |
The Ballast Configuration cluster can be used to configure a lighting ballast that restricts the light levels of a connected set of lamps. This cluster is detailed in Chapter 32. |
Parent topic:ZCL Member Clusters