Appliance statistics events
The Appliance Statistics cluster has its own events that are handled through the callback mechanism described in Chapter 3. The cluster contains its own event handler. If a device uses this cluster then application-specific Appliance Statistics event handling must be included in the user-defined callback function for the associated endpoint, where this callback function is registered through the relevant endpoint registration function. This callback function will then be invoked when an Appliance Statistics event occurs and needs the attention of the application.
For an Appliance Statistics event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_ApplianceStatisticsCallBackMessage structure:
typedef struct
{
uint8 u8CommandId;
union
{
tsCLD_ASC_LogNotificationORLogResponsePayload
*psLogNotificationORLogResponsePayload;
tsCLD_ASC_LogQueueResponseORStatisticsAvailablePayload
*psLogQueueResponseORStatisticsAvailabePayload;
tsCLD_ASC_LogRequestPayload *psLogRequestPayload;
} uMessage;
} tsCLD_ApplianceStatisticsCallBackMessage;
When an Appliance Statistics event occurs, one of four command types could have been received. The relevant command type is specified through the u8CommandId field of the tsSM_CallBackMessage structure. The possible command types are detailed the tables below for events generated on a server and a client.
u8CommandId Enumeration |
Description |
|---|---|
E_CLD_APPLIANCE_STATISTICS_ |
CMD_LOG_REQUEST
|A ‘Log Request’ message has been received by the server (appliance)| |E_CLD_APPLIANCE_STATISTICS_
CMD_LOG_QUEUE_REQUEST
|A ‘Log Queue Request’ message has been received by the server (appliance)|
u8CommandId Enumeration |
Description |
|---|---|
E_CLD_APPLIANCE_STATISTICS_ |
CMD_LOG_NOTIFICATION
|A ‘Log Notification’ message has been received by the client| |E_CLD_APPLIANCE_STATISTICS_
CMD_LOG_RESPONSE
|A ‘Log Response’ message has been received by the client| |E_CLD_APPLIANCE_STATISTICS_
CMD_LOG_QUEUE_RESPONSE
|A ‘Log Queue Response’ message has been received by the client| |E_CLD_APPLIANCE_STATISTICS_
CMD_STATISTICS_AVAILABLE
|A ‘Statistics Available’ message has been received by the client|
Parent topic:Appliance Statistics Cluster