eCLD_ASCStatisticsAvailableSend

teZCL_Status eCLD_ASCStatisticsAvailableSend(
        uint8 u8SourceEndPointId,
        uint8 u8DestinationEndPointId,
        tsZCL_Address *psDestinationAddress,
        uint8 *pu8TransactionSequenceNumber);

Description

This function can be used on an Appliance Statistics cluster server to send an unsolicited ‘Statistics Available’ message to a cluster client. The function is an alternative to eCLD_ASCLogQueueResponseORStatisticsAvailableSend().

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters

  • u8SourceEndPointId Number of the local endpoint through which to send the message. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId Number of the endpoint on the remote node to which the message is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress Pointer to a structure holding the address of the node to which the message is sent

  • pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the message

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_INVALID_VALUE

Parent topic:Functions