End Device functionality

The End Device is not capable of either forming a network or being a parent to other devices joining the network.

Two types of End Device are as follows:

  • “RX On” End Devices, which are always ready to communicate in the network

  • Sleepy “RX Off when Idle” End Devices, which can sleep for periods of time during which it cannot communicate

Note: To disable sleep on “RX Off” End Device for continuous data polling, user must define DISABLE_SLEEP in the corresponding ed_rx_off.cmake (by default, it is undefined).

The End Device supports the mandatory clusters and features of the Base Device as defined in ZigBee Base Device Behavior Specification.

For demonstrating the “Finding and Binding” functionality, the End Device also supports the On/Off cluster as a client.

All communications to/from the End Device are passed through its parent Coordinator or Router. For an RX Off with the Idle End Device, communication is initiated from the End Device through Poll Requests. The parent device then buffers data for the child End Device for some time. During this period, the End Device must send periodic Poll Requests to its parent to receive any messages that are waiting for it.

For the RX On device, no poll is required and messages are sent directly from the parent. However, regular messages must be sent. Otherwise, the device can be timed out.

Joining an existing network using network steering (ED)

A factory-new End Device can join an existing network once the network opens to accept new joiners (Network Steering for a device on a network).

Joining an existing network using Network Steering is achieved as follows:

  1. Trigger Network Steering on one of the devices already on the network.

  2. Then, reset using the RESET button or power on the End device.

Parent topic:End Device functionality

Operating the device (ED)

The operational functionality of this device in this demonstration is provided by the On/Off cluster. The device supports the On/Off cluster server. Therefore, its operation is passive and it responds to commands sent by bound devices. It responds to an OnOff Toggle command from a bound controller device, by toggling the LED1 on the FRDM-MCXW71, FRDM-MCXW72, MCX-W71-EVK, MCX-W72-EVK, RD-RW612-BGA, or the FRDM-RW612 board.

Parent topic:End Device functionality

Rejoining a network (ED)

An End Device can be restarted in a state, which is not factory-new. In such a case, it automatically sends a Network Rejoin Request to re-establish contact with its previous parent. If this fails, it then tries to join any Router on the network that can host it. The End Device attempts to rejoin when powered on and after it wakes from the deep sleep state. All the application, binding, group, and network parameters are preserved in non-volatile memory.

Parent topic:End Device functionality

Performing a factory reset (ED)

The End Device can be returned to its factory-new state (erasing all persistent data except the outgoing network frame counter) as follows:

  • Hold down the USER button and press the RESET button on the FRDM-MCXW71 board or FRDM-MCXW72 board or MCX-W71-EVK board, or MCX-W72-EVK board.

The End Device then unicasts a Leave Indication to its parent. The parent then broadcasts this message again to the old network. The End Device deletes all persistent data (other than the outgoing network frame counter) and performs a software reset.

There are two supported over-the-air commands for removing a device from the network as follows:

  • Network Leave Request without rejoin

  • ZDO Management Network Leave Request without rejoin

The Reset command of the Basic cluster causes the ZCL to be reset to its factory-state defaults. It also resets all attributes and configured reports. This step does not remove the device from the network and all network parameters, groups, and bindings remain in place.

Parent topic:End Device functionality

Parent topic:Running the demonstration examples