Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the flash.bin to the target board. Reference ‘How to get flash.bin of TrustZone examples’ Reference ‘Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf’ to make and download flash.bin.
Press the reset button on your board.
How to get flash.bin of TrustZone examples:
Create a directory named ‘tz_bin’ in your work direcory.
Build {app}_s and copy sdk2.0-app.bin into ‘tz_bin’ then rename it as sdk2.0-app_s.bin.
Build {app}_ns and copy sdk2.0-app.bin into ‘tz_bin’ then rename it as sdk2.0-app_ns.bin.
Enter the ‘tz_bin’ directory and execute ‘dd’ command to combin the two files. dd if=sdk2.0-app_ns.bin of=sdk2.0-app_s.bin bs=1 count=
ls -l ./sdk2.0-app_ns.bin|awk '{print $5}'seek=843776Rename sdk2.0-app_s.bin as m33_image.bin, and copy it into imx-mkimage
Build the corresponding flash.bin
Running the demo
The log below shows the output of the hello world demo in the terminal window:
Hello from secure world!
Entering normal world.
Welcome in normal world!
This is a text printed from normal world!
Comparing two string as a callback to normal world
String 1: Test1
String 2: Test2
Both strings are not equal!
TrustZone Application Development in SDK
Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project.
The secure project is stored in <application_name><application_name>_s directory. The non-secure project is stored in <application_name><application_name>_ns directory.
The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually ends by jump to non-secure application/project. If IDE allows the two projects in single workspace, the user can also find the project with <application_name>. This project contains both secure and non-secure projects in one workspace (Keil MDK, IAR) and it allows to user easy transition from one to another project.
Project Structure
The all TrustZone files related to TrustZone are located in trustzone virtual directory. The files are:
tzm_config.c
tzm_config.h
veneer_table.c
veneer_table.h
File tzm_config.c, tzm_config.h
This file is used by secure project only. It contains one function BOARD_InitTrustZone(), which configures complete TrustZone environment. It includes SAU, TRDC and some TrustZone related registers from System Control Block. This function is called from SystemInitHook() function, it means during system initialization.
File veneer_table.c, veneer_table.h
This file defines all secure functions (secure entry functions) exported to normal world. This file is located in secure project only. While header file is used by both secure and non-secure projects. The secure entry functions usually contain validation of all input parameters in order to avoid any data leak from secure world.
The files veneer_table.h and <application_name>_s_import_lib.o or <application_name>_s_CMSE_lib.o create the connection between secure and non-secure projects. The library file is generated by linker during compilation of secure project and it is linked to the non-secure project as any other library.
TrustZone application compilation
As first compile secure project since CMSE library is needed for compilation of non-secure project. After successful compilation of secure project, compile non-secure project.