Hardware requirements
Mini/micro USB cable
EVB-MIMXRT1050 board
Personal Computer
Board settings
Make sure nand flash is avaliable on board.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like below, after shell is avaliable, please start with command “help”.
nand flash management demo.
Make file system..............
Create directory......
SHELL (build: Feb 11 2018)
Copyright 2017 NXP
SHELL>>