Hardware requirements
Mini/micro USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the eRPC Matrix Multiply RTOS demo in the terminal window:
Primary core started
Copy CORE1 image to address: 0x303C0000, size: 15548
Matrix #1
=========
21 33 37 37 9
23 45 43 0 32
38 44 8 15 36
18 18 38 44 16
22 23 0 38 7
Matrix #2
=========
11 23 27 45 11
7 19 23 24 6
32 26 49 43 16
22 48 36 34 41
27 20 32 31 11
eRPC request is sent to the server
Result matrix
=============
2703 4028 4759 4865 2637
2808 3142 4787 4956 1563
2284 3358 4122 4736 1821
2940 4176 4858 4868 2894
1428 2907 2715 3051 2015
Press the SW8 button to initiate the next matrix multiplication
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.
Note: FRDM-IMXRT1186 GPIO_AON_04 pin is shared between SW8 button and headphone HP_DET_B pin. Once a headphone is inserted into J101 Audio Jack connector the SW8 button functionality is affected, causing eRPC request are triggered repeatedly without the button being pressed. Please remove the headphone in this case.