Hardware requirements

  • Type-C USB cable

  • FRDM-MCXA156 Board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows:

SLAVE(FlexIO SPI)          connect to      MASTER(LPSPI0)
Pin Name   Board Location                   Pin Name    Board Location
SOUT       J8 pin 14                       SIN         J6 pin 5
SIN        J8 pin 13                       SOUT        J6 pin 6
SCK        J8 pin 15                       SCK         J6 pin 4
PCS0       J8 pin 16                       PCS0        J6 pin 3

Prepare the Demo

  1. Connect a USB cable between the host PC and the EVK board J21.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

LPSPI Master interrupt - FLEXIO SPI Slave edma example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master uses interrupt and slave uses edma way.
Please make sure you make the correct line connection. Basically, the connection is: 
LPSPI_master -- FLEXIO_SPI_slave   
   CLK      --    CLK  
   PCS      --    PCS  
   SOUT     --    SIN  
   SIN      --    SOUT 
This is FLEXIO SPI slave call back.
LPSPI master <-> FLEXIO SPI slave transfer all data matched!

End of Example.