Hardware requirements
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ERM error recording example.
Original ram data correct.
ERM error recording address is 0x20000000.
ERM error recording example finished successfully.
Note: All system bus masters can access the programming model:
Only in supervisor mode
Using only 32-bit (word) accesses Any of the following attempted references to the programming model generates an error termination:
In user mode
Using non-32-bit access sizes
To undefined (reserved) addresses