Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
MASTER(LPSPI3) connect to SLAVE(FlexIO SPI)
Pin Name Board Location Pin Name Board Location
SOUT J2 pin 10 SIN J8 pin 26
SIN J2 pin 8 SOUT J8 pin 25
SCK J2 pin 12 SCK J8 pin 27
PCS0 J2 pin 6 PCS0 J8 pin 28
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
LPSPI Master interrupt - FLEXIO SPI Slave edma example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master uses interrupt and slave uses edma way.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is FLEXIO SPI slave call back.
LPSPI master <-> FLEXIO SPI slave transfer all data matched!
End of Example.