Hardware requirements
USB Type-C cable
i.MX943-EVK board
Personal Computer
Power supply 24V
Motor control board (FRDM-LVPMSM-FA)
EnDat3 sensor
Board settings
Insert FRDM-LVPMSM-FA board into Arduino interface of motor control 2. Connect EnDat3 sensor and power supply to FRDM-LVPMSM-FA
EnDat3 connection:
INSTANCE(FRDM-LVPMSM-FA)  CONNECTS TO  INSTANCE(EnDat2.2 sensor)
Pin Name        Board Location              Signal Name
ENC_DATA_IO_P      J70-4                     DATA_P
ENC_DATA_IO_N      J70-9                     DATA_N
VENC               J70-1                     UP - Power supply voltage
GND                J70-6                     GND
SW90 setting:
SW[1-2] OFF:ON Half duplex
SW[3]   OFF    Echo Enabled
SW[4]   ON     ENDAT is used.
SW30 setting - Select the appropriate voltage based on the properties of the sensor
SW[1] ON 3.3V
SW[2] ON 5.2V
SW[3] ON 9V
SW[4] ON 12V
Jumpers:
J300: pin1 <--> pin2
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.
Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.