Hardware requirements
Micro USB cable
LPCXpresso55S28 board
Personal Computer
Board settings
    Master_board(SPI7)           Slave_board(SPI2)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       P17  pin 12         MISO      P18  pin 6
MOSI       P17  pin 10         MOSI      P18  pin 10
SCK        P17  pin 14         SCK       P18  pin 8
SSEL1      P17  pin 1          SSEL0     P17  pin 16
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~