Hardware requirements
Micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the LPC-Link USB port (P6) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project. Running the demo =============== When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
Usart waking up soc from deep sleep example, please note USART can only work at 9600 baudrate in deep sleep mode
Press 1 to enter deep sleep
Press any other key to wake up soc
/* Type in '1' into UART terminal */
Received 1
Entering deep sleep mode, please change the baudrate setting of your local terminal to 9600
/* Type in '2' into UART terminal */
Received 2
Waking up from deep sleep, please change the baudrate setting of your local terminal back to 115200