erpc_two_way_rpc_rpmsg_rtos
Overview
The Multicore eRPC Two Way RPC RTOS project is a simple demonstration program that uses the MCUXpresso SDK software and the Multicore SDK to show how to implement the Remote Procedure Call between cores of the multicore system.
This multicore example shows how both the eRPC client and the eRPC server can be setup on one side/core (bidirectional communication) and how to handle callback functions in eRPC.
The primary core (Core0) creates client and server tasks first. The client task releases the secondary core from the reset, initializes the RPMsg-Lite erpc transport and once the server task is running it configures the arbitrated client. Then the application logic is running.
The secondary core (Core1) creates client and server tasks two. The client task initializes the RPMsg-Lite erpc transport and once the server task is running it configures the arbitrated client. Then the application logic is running. The client task logic of the Core1 is very simple, it repeatedly calls the increaseNumber() erpc function that is implemented on the Core0 and that increments the counter.
The client task logic of the Core0 alternately issues either getNumberFromCore0() function implementation on the Core0 or getNumberFromCore1() function implementation on the Core1 (erpc call). Then, the nestedCallGetNumber() erpc function call is issued that alternately triggers either getNumberFromCore1() function implementation on the Core1 (normal erpc call) or it triggers the getNumberFromCore0() function implementation on the Core0 (nested erpc call, routed through the Core1 erpc server).
eRPC documentation
eRPC specific files are stored in: middleware\multicore\erpc eRPC documentation is stored in: middleware\multicore\erpc\doc eRPC is open-source project stored on github: https://github.com/EmbeddedRPC/erpc eRPC documentation can be also found in: http://embeddedrpc.github.io
Building the application
This shows example how to build application for evkbmimxrt1170 board with cm7 core_id.
Change the -b <board> parameter based on board you want to build.
Change the -Dcore_id=<core_id> parameter based on board core you want to build.
For these parameters please see attribute boards: in primary/example.yml.
west build --sysbuild examples/multicore_examples/erpc_two_way_rpc_rpmsg_rtos/primary --toolchain armgcc --config debug -b evkbmimxrt1170 -Dcore_id=cm7