rpmsg_lite_pingpong_rtos_no_mcmgr
Overview
The Multicore RPMsg-Lite pingpong FreeRTOS project is a simple demonstration program that uses the MCUXpresso SDK software and the RPMsg-Lite library and shows how to implement the inter-core communication between cores of the multicore system without multicore manager.
Once the RPMsg is initialized and endpoints are created the message exchange starts, incrementing a virtual counter that is part of the message payload.
The message pingpong finishes when the counter reaches the value of 100. Then the RPMsg-Lite is deinitialized and the procedure of the data exchange is repeated again.
Building the application
This shows example how to build application for imx943evk board with cm7_core1 and cm33_core1 core_id.
Change the -b <board> parameter based on board you want to build.
Change the -Dcore_id=<core_id> parameter based on board core you want to build.
For these parameters please see attribute boards: in master/example.yml and remote/example.yml.
west build examples/multicore_examples/rpmsg_lite_pingpong_rtos_no_mcmgr/master --toolchain armgcc --config debug -b imx943evk -Dcore_id=cm7_core1
west build examples/multicore_examples/rpmsg_lite_pingpong_rtos_no_mcmgr/remote --toolchain armgcc --config debug -b imx943evk -Dcore_id=cm33_core1