dev_printer_virtual_plain_text
Overview
The USB virtual printer application is a simple application to demonstrate a virtual printer functionality. Because there is no printer language parsing, the received raw data is output directly in the debug console. As a result, only plain text is suitable for testing. For other printer language support, such as postscript, implement the corresponding parser.
System Requirements
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements
The project files for lite version examples are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_printer_virtual_plain_text_lite/ / . 
For non-lite version example, the path is:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_printer_virtual_plain_text/ / . 
The
is Bare Metal or FreeRTOS OS. 
Getting Started
Hardware Settings
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Download the program to the target board.
Connect the target board to the external power source (the example is self-powered).
Power off the target board. Then power on again.
Connect a USB cable between the PC and the USB device port of the board.
For detailed instructions, see the appropriate board User’s Guide.
Run the example on Windows7
Plug in the device, which is running the printer example, into the PC.
Wait for the PC to auto-install the driver. When the PC completes the installation, no driver is found as follows:
Opening the device manager, these devices are shown:

Test generic printer driver. Right click the device in “Other devices” group, select “Update Driver Software…”, select “Browse my computer for driver software”, select “Let me pick from a list of device drivers on my computer”, select “Printers”, select “Generic” & “Generic / Text Only”, and click on “Next” and “Yes” to install.

After installing the driver, the “Generic / Text Only” printer is available in the “Devices and Printers”
Print one text file using this printer.
The debug console data is as follows:

Run the example on Windows10
Plug in the device, which is running the printer example, into the PC.
Wait for the PC to auto-install the driver. When the PC completes the installation, opening the device manager, these devices are shown:

Right click on the NXPksdk printer demo and select “Properties”, in the pop-up window, select the “Events” and find the configured port.

In Control Panel, open the “Devices and Printers” window, click “Add a printer”.

In pop-up window, select “The printer that I want isn’t listed”, select “Add a local printer or network printer with manual settings”, select the port that showed in previous “Events” tab, select “Generic” & “Generic / Text Only”, select “use the driver that is currently installed”, and click on “Next” and “Yes” to install.

After above steps, a “Generic/Text Only” printer is available in “Devices and Printers”.
Print one text file using this printer.
The debug console data is as follows:

Test postscript printer driver. Right click the “USB printing Support” and select “Uninstall”. Unplug and plug in again.
Wait for the PC to install the driver as in step 2.
In Control Panel, open the “Devices and Printers” window, click “Add a printer”, In pop-up window, select “The printer that I want isn’t listed”, select “Add a local printer or network printer with manual settings”, select the port that showed in previous “Events” tab, select “Microsoft” & “Microsoft PS Class Driver”, select “use the driver that is currently installed”, and click on “Next” and “Yes” to install.
Print one text file using this printer. For example, if printing the same file as in step 7, the postscript data is displayed in the debug console. The demo does not parse the data and outputs it to the debug console directly.
*/
Supported Boards
MIMXRT1170-EVKB
FRDM-K22F
LPCXpresso55S69
EVK-MIMXRT1064
FRDM-MCXA153
MIMXRT685-AUD-EVK
LPCXpresso51U68
LPCXpresso54S018
LPCXpresso55S16
LPCXpresso54S018M
MIMXRT1060-EVKB
EVK-MIMXRT1010
MIMXRT1040-EVK
FRDM-MCXN947
MIMXRT1024-EVK
LPCXpresso55S28
LPCXpresso54628
LPCXpresso55S36
MCX-N5XX-EVK
MIMXRT1060-EVKC
MIMXRT1160-EVK
MIMXRT1180-EVK
FRDM-K32L2A4S
EVK-MIMXRT1020
MIMXRT700-EVK
FRDM-MCXA156
EVK-MIMXRT595
EVK-MIMXRT685
MCX-N9XX-EVK
EVKB-IMXRT1050
RD-RW612-BGA
FRDM-K32L3A6
EVK-MIMXRT1015
FRDM-MCXN236
FRDM-RW612