Scanning
The most basic setup for a Central device begins with scanning, which is performed by the following function from gap_interface.h:
bleResult_t Gap_StartScanning
(
const gapScanningParameters_t* pScanningParameters,
gapScanningCallback_t scanningCallback,
gapFilterDuplicates_t enableFilterDuplicates,
uint16_t duration,
uint16_t period
);
If the pScanningParameters pointer is NULL, the currently set parameters are used. If no parameters have been set after a device power-up, the standard default values are used:
#define gGapDefaultScanningParameters_d \
{ \
/* type */ gGapScanTypePassive_c, \
/* interval */ gGapScanIntervalDefault_d, \
/* window */ gGapScanWindowDefault_d, \
/* ownAddressType */ gBleAddrTypePublic_c, \
/* filterPolicy */ gScanAll_c \
/* scanning PHY */ gLePhylMFlag_c\
}
The easiest way to define non-default scanning parameters is to initialize a gapScanningParameters_t structure with the above default and change only the required fields.
For example, to perform active scanning and only scan for devices in the Filter Accept List, the following code can be used:
gapScanningParameters_t scanningParameters = gGapDefaultScanningParameters_d;
scanningParameters.type = gGapScanTypeActive_c;
scanningParameters.filterPolicy = gScanWithFilterAcceptList_c;
Gap_StartScanning(&scanningParamters, scanningCallback, enableFilterDuplicates, duration, period);
When using the common application structure, the application can use the following API defined in app_conn.h:
bleResult_t BluetoothLEHost_StartScanning
(
appScanningParams_t *pAppScanParams,
gapScanningCallback_t pfCallback
);
The API uses the appScanningParams_t structure, which is defined as follows:
typedef struct appScanningParams_tag
{
gapScanningParameters_t *pHostScanParams; /*!< Pointer to host scan structure */
gapFilterDuplicates_t enableDuplicateFiltering; /*!< Duplicate filtering mode */
uint16_t duration; /*!< scan duration */
uint16_t period; /*!< scan period */
} appScanningParams_t;
The scanningCallback is triggered by the GAP layer to signal events related to scanning.
The most important event is the gDeviceScanned_c event, which is triggered each time an advertising device is scanned. This event data contains information about the advertiser:
typedef struct
{
bleAddressType_t addressType ;
bleDeviceAddress_t aAddress ;
int8_t rssi ;
uint8_t dataLength ;
uint8_t* data ;
bleAdvertisingReportEventType_t advEventType ;
bool_t directRpaUsed;
bleDeviceAddress_t directRpa;
bool_t advertisingAddressResolved;
} gapScannedDevice_t;
If this information signals a known Peripheral that the Central wants to connect to, the latter must stop scanning and connect to the Peripheral.
To stop scanning, call this function:
bleResult_t Gap_StopScanning (void);
By default, the GAP layer is configured to report all scanned devices to the application using the gDeviceScanned_c event type. However, some use cases might require to perform specific GAP Discovery Procedures. In such use cases the advertising reports might require the filtering of Flags AD value from the advertising data. Other use cases require the Bluetooth LE Host Stack to automatically initiate a connection when a specific device has been scanned.
To enable filtering based on the Flags AD value or to set device addresses for automatic connections, the following function must be called before the scanning is started:
bleResult_t Gap_SetScanMode
(
gapScanMode_t scanMode,
gapAutoConnectParams_t* pAutoConnectParams,
gapConnectionCallback_t connCallback
);
The default value for the scan mode is gDefaultScan_c, which reports all packets regardless of their content and does not perform any automatic connection.
To enable Limited Discovery, the gLimitedDiscovery_c value must be used, while the gGeneralDiscovery_c value activates General Discovery.
To enable automatic connection when specific devices are scanned, the gAutoConnect_c value must be set, in which case the pAutoConnectParams parameter must point to the structure that holds the target device addresses and the connection parameters to be used by the Host for these devices.
If scanMode is set to gAutoConnect_c, connCallback must be set and is triggered by GAP to send the events related to the connection.
Parent topic:Central setup