Intrusion Detection System
The Intrusion Detection System (IDS) is a proprietary feature which allows the Car Anchor to monitor anomalous events related to the traffic and conditions generated during the operation of the Bluetooth LE software stack. These events are detected at Host and Controller level. The application registers a callback where it receives and handles reports.
The IDS feature is supported on the following platforms:
KW45B41Z-EVK
KW47-EVK
To enable IDS, modify the Digital Key Car Anchor as per the steps listed below:
Update the application project so that it uses the experimental Bluetooth LE Host library path:
middleware/wireless/bluetooth/host/lib_exp/.In
app_preinclude.hfile, setgIntrusionDetectionSystem_dtoTRUE.