Development platform
MCUXpresso
NXP MCUXpresso provides an Eclipse-based platform for developing applications for the JN518x and K32W041/K32W061/K32W1/MCXW71/MCXW72 devices. This platform can be obtained from https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide and must be a registered edition. The required version of MCUXpresso is indicated in the Release Notes for the ZigBee 3.0 SDK.
For installation and operational instructions, first refer to the MCUXpresso Installation and User Guide. More detailed operational instructions are provided in the MCUXpresso User Guide, available from the above website.
Attention: Zigbee applications on RW612 platform do not support MCUXPresso IDE projects. Instead they are built with the west tool, refer to the https://github.com/nxp-mcuxpresso/mcux-sdk for more information.
Parent topic:Development platform
Parent topic:Development environment and resources