ZPS_eAplZdpNwkAddrRequest
ZPS\_teStatus ZPS\_eAplZdpNwkAddrRequest\(
PDUM\_thAPduInstance hAPduInst,
ZPS\_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS\_tsAplZdpNwkAddrReq *psZdpNwkAddrReq);
Description
This function requests the 16-bit network address of the node with a particular 64-bit IEEE (MAC) address. The function sends out an NWK_addr_req request, which can be either unicast or broadcast, as follows:
Unicast to another node, specified through uDstAddr, that will ‘know’ the required network address (this may be the parent of the node of interest or the Coordinator)
Broadcast to the network, in which case uDstAddrmust be set to the special network address 0xFFFF (see Section 9.3)
The IEEE address of the node of interest must be specified in the request, represented by the structure below (detailed further in Section 9.2.2.1).
typedef struct {
uint64 u64IeeeAddr;
uint8 u8RequestType;
uint8 u8StartIndex;
} ZPS_tsAplZdpNwkAddrReq;
The required network address is received in an NWK_addr_resp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpNwkAddrRsp(detailed in Section 9.2.3.1). Note that this response can optionally contain the network addresses of the responding node’s neighbors (this option is selected as part of the request through u8RequestType).
Parent topic:ZPS_eAplZdpNwkAddrRequest
Parameters
hAPduInst: Handle of APDU instance in which request is sent
uDstAddr: Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)
bExtAddr: Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
*pu8SeqNumber: Pointer to sequence number of request
*psZdpNwkAddrReq: Pointer to request (see above).
Parent topic:ZPS_eAplZdpNwkAddrRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpNwkAddrRequest
Parent topic:Address discovery functions