Device Structure
The following tsZLO_OccupancySensorDevice structure is the shared structure for an Occupancy Sensor device:
typedef struct
{
tsZCL_EndPointDefinition sEndPoint;
/* Cluster instances */
tsZLO_OccupancySensorDeviceClusterInstances sClusterInstance;
/* Mandatory server clusters */
#if (defined CLD_BASIC) && (defined BASIC_SERVER)
/* Basic Cluster - Server */
tsCLD_Basic sBasicServerCluster;
#endif
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
/* Identify Cluster - Server */
tsCLD_Identify sIdentifyServerCluster;
tsCLD_IdentifyCustomDataStructure sIdentifyServerCustomDataStructure;
#endif
#if (defined CLD_OCCUPANCY_SENSING) && (defined OCCUPANCY_SENSING_SERVER)
/* Occupancy Sensing Cluster - Server */
tsCLD_OccupancySensing sOccupancySensingServerCluster;
#endif
/* Optional server clusters */
#if (defined CLD_POLL_CONTROL) && (defined POLL_CONTROL_SERVER)
tsCLD_PollControl sPollControlServerCluster;
tsCLD_PollControlCustomDataStructure
sPollControlServerCustomDataStructure;
#endif
/* Mandatory client clusters */
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_CLIENT)
/* Identify Cluster - Client */
tsCLD_Identify sIdentifyClientCluster;
tsCLD_IdentifyCustomDataStructure sIdentifyClientCustomDataStructure;
#endif
/* Recommended Optional client clusters */
#if (defined CLD_POLL_CONTROL) && (defined POLL_CONTROL_CLIENT)
tsCLD_PollControl sPollControlClientCluster;
tsCLD_PollControlCustomDataStructure
sPollControlClientCustomDataStructure;
#endif
#if (defined CLD_GROUPS) && (defined GROUPS_CLIENT)
/* Groups Cluster - Client */
tsCLD_Groups sGroupsClientCluster;
tsCLD_GroupsCustomDataStructure sGroupsClientCustomDataStructure;
#endif
#if (defined CLD_OTA) && (defined OTA_CLIENT)
tsCLD_AS_Ota sCLD_OTA;
tsOTA_Common sCLD_OTA_CustomDataStruct;
#endif
} tsZLO_OccupancySensorDevice;;
Parent topic:Occupancy Sensor