Device Structure
The following tsZLO_OnOffBallastDevice structure is the shared structure for an On/Off Ballast device:
typedef struct
{
tsZCL_EndPointDefinition sEndPoint;
/* Cluster instances */
tsZLO_OnOffBallastDeviceClusterInstances sClusterInstance;
/* Mandatory server clusters */
#if (defined CLD_BASIC) && (defined BASIC_SERVER)
/* Basic Cluster - Server */
tsCLD_Basic sBasicServerCluster;
#endif
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
/* Identify Cluster - Server */
tsCLD_Identify sIdentifyServerCluster;
tsCLD_IdentifyCustomDataStructure
sIdentifyServerCustomDataStructure;
#endif
#if (defined CLD_ONOFF) && (defined ONOFF_SERVER)
/* On/Off Cluster - Server */
tsCLD_OnOff sOnOffServerCluster;
tsCLD_OnOffCustomDataStructure sOnOffServerCustomDataStructure;
#endif
#if (defined CLD_SCENES) && (defined SCENES_SERVER)
/* Scenes Cluster - Server */
tsCLD_Scenes sScenesServerCluster;
tsCLD_ScenesCustomDataStructure sScenesServerCustomDataStructure;
#endif
#if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
/* Groups Cluster - Server */
tsCLD_Groups sGroupsServerCluster;
tsCLD_GroupsCustomDataStructure sGroupsServerCustomDataStructure;
#endif
/* Optional server clusters */
#if (defined CLD_POWER_CONFIGURATION) && (defined
POWER_CONFIGURATION_SERVER)
/* Power Configuration Cluster - Server */
tsCLD_PowerConfiguration sPowerConfigServerCluster;
#endif
#if (defined CLD_DEVICE_TEMPERATURE_CONFIGURATION) && (defined
DEVICE_TEMPERATURE_CONFIGURATION_SERVER)
/* Device Temperature Configuration Cluster - Server */
tsCLD_DeviceTemperatureConfiguration
sDeviceTemperatureConfigurationServerCluster;
#endif
#if (defined CLD_BALLAST_CONFIGURATION) && (defined
BALLAST_CONFIGURATION_SERVER)
tsCLD_BallastConfiguration sBallastConfigurationServerCluster;
#endif
/* Recommended Optional server clusters */
#if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_SERVER)
/* LevelControl Cluster - Server */
tsCLD_LevelControl sLevelControlServerCluster;
tsCLD_LevelControlCustomDataStructure
sLevelControlServerCustomDataStructure;
#endif
#if (defined CLD_ILLUMINANCE_LEVEL_SENSING) && (defined
ILLUMINANCE_LEVEL_SENSING_SERVER)
tsCLD_IlluminanceLevelSensing
sIlluminanceLevelSensingServerCluster;
#endif
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
tsCLD_ZllCommission sZllCommissionServerCluster;
tsCLD_ZllCommissionCustomDataStructure
sZllCommissionServerCustomDataStructure;
#endif
/*Recommended Optional client clusters */
#if (defined CLD_OTA) && (defined OTA_CLIENT)
/* OTA cluster - Client */
tsCLD_AS_Ota sCLD_OTA;
tsOTA_Common sCLD_OTA_CustomDataStruct;
#endif
#if (defined CLD_ILLUMINANCE_MEASUREMENT) && (defined
ILLUMINANCE_MEASUREMENT_CLIENT)
/* Illuminance Measurement Cluster - Client */
tsCLD_IlluminanceMeasurement sIlluminanceMeasurementClientCluster;
#endif
#if (defined CLD_ILLUMINANCE_LEVEL_SENSING) && (defined
ILLUMINANCE_LEVEL_SENSING_CLIENT)
tsCLD_IlluminanceLevelSensing
sIlluminanceLevelSensingClientCluster;
#endif
#if (defined CLD_OCCUPANCY_SENSING) && (defined
OCCUPANCY_SENSING_CLIENT)
/* Occupancy Sensing Cluster - Client */
tsCLD_OccupancySensing sOccupancySensingClientCluster;
#endif
} tsZLO_OnOffBallastDevice;
Parent topic:On/Off Ballast