Device structure
The following tsZLO_OnOffSensorDevice structure is the shared structure for a On/Off Sensor device:
typedef struct
{
tsZCL_EndPointDefinition sEndPoint;
/* Cluster instances */
tsZLO_OnOffSensorDeviceClusterInstances sClusterInstance;
#if (defined CLD_BASIC) && (defined BASIC_SERVER)
/* Basic Cluster - Server */
tsCLD_Basic sBasicServerCluster;
#endif
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
/* Identify Cluster - Server */
tsCLD_Identify sIdentifyServerCluster;
tsCLD_IdentifyCustomDataStructure
sIdentifyServerCustomDataStructure;
#endif
/* Recommended Optional Server Cluster */
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
tsCLD_ZllCommission sZllCommissionServerCluster;
tsCLD_ZllCommissionCustomDataStructure
sZllCommissionServerCustomDataStructure;
#endif
/** Mandatory client clusters*/
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_CLIENT)
/* Identify Cluster - Client */
tsCLD_Identify sIdentifyClientCluster;
tsCLD_IdentifyCustomDataStructure
sIdentifyClientCustomDataStructure;
#endif
#if (defined CLD_ONOFF) && (defined ONOFF_CLIENT)
/* On/Off Cluster - Client */
tsCLD_OnOff sOnOffClientCluster;
#endif
/* Recommended Optional Client CLuster */
#if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_CLIENT)
/* Level Control Cluster - Client */
tsCLD_LevelControl sLevelControlClientCluster;
tsCLD_LevelControlCustomDataStructure
sLevelControlClientCustomDataStructure;
#endif
#if (defined CLD_SCENES) && (defined SCENES_CLIENT)
/* Scenes Cluster - Client */
tsCLD_Scenes sScenesClientCluster;
tsCLD_ScenesCustomDataStructure sScenesClientCustomDataStructure;
#endif
#if (defined CLD_GROUPS) && (defined GROUPS_CLIENT)
/* Groups Cluster - Client */
tsCLD_Groups sGroupsClientCluster;
tsCLD_GroupsCustomDataStructure sGroupsClientCustomDataStructure;
#endif
#if (defined CLD_COLOUR_CONTROL) && (defined COLOUR_CONTROL_CLIENT)
/* Colour Control Cluster - Client */
tsCLD_ColourControl sColourControlClientCluster;
tsCLD_ColourControlCustomDataStructure
sColourControlClientCustomDataStructure;
#endif
#if (defined CLD_OTA) && (defined OTA_CLIENT)
/* OTA cluster - Client */
tsCLD_AS_Ota sCLD_OTA;
tsOTA_Common sCLD_OTA_CustomDataStruct;
#endif
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_CLIENT)
tsCLD_ZllCommission sZllCommissionClientCluster;
tsCLD_ZllCommissionCustomDataStructure
sZllCommissionClientCustomDataStructure;
#endif
} tsZLO_OnOffSensorDevice;
Parent topic:On/Off Sensor