Registration Function
The following eZLO_RegisterColourTemperatureLightEndPoint() function is the endpoint registration function for a color Temperature Light device.
teZCL_Status eZLO_RegisterColourTemperatureLightEndPoint(
uint8 u8EndPointIdentifier,
tfpZCL_ZCLCallBackFunction cbCallBack,
tsZLO_ColourTemperatureLightDevice *psDeviceInfo);
Description
This function is used to register an endpoint which supports a color Temperature Light device. The function must be called after eZCL_Initialise().
The specified identifier for the endpoint is a number in the range 1 to 240 (endpoint 0 is reserved for ZigBee use). Application endpoints are normally numbered consecutively starting at 1. The specified number must be less than or equal to the value of ZLO_NUMBER_OF_ENDPOINTS defined in the zcl_options.h file, which represents the highest endpoint number used for applications.
While invoking this function, specify a user-defined callback function, which is invoked when an event associated with the endpoint occurs. This callback function is defined according to the typedef:
typedef void(* tfpZCL_ZCLCallBackFunction)
(tsZCL_CallBackEvent *pCallBackEvent);
Also provide a pointer to a tsZLO_ColourTemperatureLightDevice structure, described in Device Structure. This structure stores all variables relating to the color Controller device associated with the endpoint. The sEndPoint and sClusterInstance fields of this structure are set by this function and must not be directly written to by the application.
The function is called multiple times if more than one endpoint is being used - for example, if more than one color Temperature Light device is housed in the same hardware, sharing the same module.
Parameters
u8EndPointIdentifier: Endpoint that is to be associated with the registered structure and callback function.
cbCallBack: Pointer to the function that is used to indicate events to the application for this endpoint.
psDeviceInfo: Pointer to the structure that acts as storage for all variables related to the device being registered on this endpoint (see Device Structure). The
sEndPointandsClusterInstancefields are set by this register function for internal use and must not be written to by the application.
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_PARAMETER_RANGE
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_CLUSTER_0
E_ZCL_ERR_CALLBACK_NULL
E_ZCL_ERR_CLUSTER_NULL
E_ZCL_ERR_SECURITY_RANGE
E_ZCL_ERR_CLUSTER_ID_RANGE
E_ZCL_ERR_MANUFACTURER_SPECIFIC
E_ZCL_ERR_ATTRIBUTE_TYPE_UNSUPPORTED
E_ZCL_ERR_ATTRIBUTE_ID_ORDER
E_ZCL_ERR_ATTRIBUTES_ACCESS
The above codes are described in the ZCL User Guide (JNUG3132).
Parent topic:Colour Temperature Light