Building Applications
The server and client applications must be built with the makefiles adapted for OTA upgrade (see Section 49.14.1). A build can be conducted from MCUXpresso as for any ZigBee PRO application - refer to the MCUXpresso Installation and User Guide (JNUG3136).
The resulting binary files must then be prepared and loaded into Flash memory as described in Section 49.14.3 and Section 49.14.4.
Parent topic:Build Process