eOTA_ClientQuerySpecificFileRequest
eOTA_ClientQuerySpecificFileRequest(
uint8 u8SourceEndpoint,
uint8 u8DestinationEndpoint,
tsZCL_Address *psDestinationAddress,
tsOTA_QuerySpecificFileRequestPayload
*psQuerySpecificFileRequestPayload);
Description
This function can be used to issue a Query Specific File Request to the server. It should be called to request a device-specific file from the server. As a result of this function call, a Query Specific File Response will (eventually) be received in reply.
Parameters
u8SourceEndpoint: Number of endpoint (on client) from which the request is sent
u8DestinationEndpoint: Number of endpoint (on server) to which the request is sent
psDestinationAddress: Pointer to structure containing the address of the target server
psQuerySpecificFileRequestPayload: Pointer to structure containing payload for Query Specific File Request
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Client Functions