eOTA_HandleImageVerification

teZCL_Status eOTA_HandleImageVerification(
    uint8 u8SourceEndPointId,
    uint8 u8DstEndpoint,
    teZCL_Status eImageVerificationStatus);

Description

This function transmits an upgrade end request with the specified status.

Parameters

  • u8SourceEndPointId: Identifier of endpoint on which the cluster client operates

  • u8DstEndpoint: Identifier of endpoint (on the server) to which the upgrade end request is sent

  • eImageVerificationStatus: Image status code

Returns

  • E_ZCL_FAIL

  • E_ZCL_SUCCESS

Parent topic:Client Functions