eOTA_SpecificFileUpgradeEndRequest
eOTA_SpecificFileUpgradeEndRequest(
uint8 u8SourceEndPointId,
uint8 u8Status);
Description
This function can be used to issue an Upgrade End Request for the device-specific file download that is in progress in order to indicate to the server that the download has completed. This request can be issued by the client optionally after the downloaded image has been verified and found to be valid.
Parameters
u8SourceEndPointId: Number of endpoint (on client) from which the request is sent
u8Status: Download status of device-specific file - if the file has been completely and successfully received, this parameter must be set to OTA_STATUS_SUCCESS
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Client Functions