vOTA_SetImageValidityFlag

void vOTA_SetImageValidityFlag(
    uint8 u8Location,
    tsOTA_Common *psCustomData,
    bool bSet,
    tsZCL_EndPointDefinition *psEndPointDefinition);

Description

This function can be used to set an image validity flag once a downloaded upgrade image has been received and verified by the client.

Parameters

  • u8Location: Number of sector where image starts in Flash memory

  • psCustomData: Pointer to custom data for image (see Section 49.11.2)

  • bSet: Flag state to be set:

  • TRUE - Reset

  • FALSE - No reset

  • psEndPointDefinition: Pointer to endpoint definition (see Section 6.1.1)

Returns

  • None

Parent topic:Client Functions