Logo
25.09.02
MCUXpresso SDK Project v: latest
Document Release Versions
25.09.02
25.09.00
25.06.00
latest
  • Getting Started & Release Notes
  • Drivers
  • Middleware
    • Boot
    • Cloud
    • Connectivity
    • eIQ
      • eIQ
        • TensorFlow Lite Library For Micro User's Guide
          • Overview
          • TensorFlow Lite for Microcontrollers
          • Build Status
          • Contributing
          • Getting Help
          • Additional Documentation
          • RFCs
          • Deployment
          • Example applications
          • Model Conversion to TensorFlow Lite Format
          • Model Conversion for NXP eIQ Neutron NPU
          • Example: Converting a Quantized TensorFlow Lite Model for Neutron NPU
          • Run and debug eIQ HiFi4 and HiFi1 DSP examples using Xplorer IDE
          • Running an inference
          • Code size optimization
          • Note about the source code in the document
        • Media Processing Pipeline User's Guide
        • ExecuTorch User's Guide
    • File System
    • Motor Control
    • MultiCore
    • Wireless
  • RTOS
mcuxsdk
  • Docs »
  • Middleware »
  • eIQ »
  • eIQ »
  • eIQ TensorFlow Lite for Micro Library User Guide
  • Open on Repo Report an issue

eIQ TensorFlow Lite for Micro Library User Guide

Table of Contents

  • Overview
  • TensorFlow Lite for Microcontrollers
  • Build Status
    • Official Builds
    • Community Supported TFLM Examples
    • Community Supported Kernels and Unit Tests
  • Contributing
  • Getting Help
  • Additional Documentation
  • RFCs
  • Deployment
  • Example applications
  • Model Conversion to TensorFlow Lite Format
  • Model Conversion for NXP eIQ Neutron NPU
  • Example: Converting a Quantized TensorFlow Lite Model for Neutron NPU
  • Run and debug eIQ HiFi4 and HiFi1 DSP examples using Xplorer IDE
    • Prepare CM33 Core for the examples
    • Prepare DSP core for the examples
  • Running an inference
    • Converting a model to a C language header file {#EXAMPLE_4 .section}
    • NPU inference {#npu_infer .section}
    • Adjusting the tensor arena size {#adjust_arena .section}
  • Code size optimization
    • Register only used operators in TensorFlow Lite Micro {#SECTION_SS1_DJQ_QPB .section}
  • Note about the source code in the document

Copyright 2025, NXP. Last generated on Jun 23, 2026 11:48+0200; branch release/25.09.02, revision b735774e6343fafb3417af46f7e5a0b95170a86d.