Xtensa Software Tools Platform Support

The Xtensa Software Tools are officially supported on the following platforms:

  • **Windows:**Win 10 64-bit, Win 8 64-bit, Win 7 64-bit

  • **Linux:**RHEL 6 64-bit (with ‘Desktop’ package installed)

There may be compatibility issues with other versions of Linux or Windows, especially when using the IDE. Also note that security-enhanced Linux (SELinux) is not a supported platform because the OS can prevent different shared libraries (including Xtensa Tools) from loading.

For details on platform support and installation guidelines, see the Xtensa Development Tools Installation Guide.

Parent topic:Install Xplorer Toolchains