Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
I3C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of I3C interface, I3C0 pins of MASTER_BOARD are connected with I3C0 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
I3C0_SCL/P1_9 J8-3 P1_9 J8-3
I3C0_SDA/P1_8 J8-4 P1_8 J8-4
GND J5-8 GND J5-8
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Press reset button to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
I3C bus master example.
I3C bus master creates.
I3C bus mastership handoff.