Hardware requirements

  • Micro USB cable

  • IMX95LP4X-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

The Multicore RPMsg-Lite string echo project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.

Prepare the Demo

  1. Connect a micro USB cable between the host PC and the J31 USB port on the target board. Open two serial terminals for A Core and M Core with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control (e.g. /dev/ttyUSB0~3, /dev/ttyUSB2 for A Core, /dev/ttyUSB3 for M Core)

  2. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board

  3. Make flash.bin and burn it to imx95(refer to Getting_Started_with_MCUXpresso_SDK_for_IMX95LP4XEVK_review.pdf)

  4. Boot to linux.

  5. After login, make sure imx_rpmsg_tty kernel module is inserted (lsmod) or insert it (modprobe imx_rpmsg_tty).

Running the demo

After the boot process succeeds, the ARM Cortex-M33 terminal displays the following information:

RPMSG String Echo FreeRTOS RTOS API Demo...

Nameservice sent, ready for incoming messages...

After the Linux RPMsg tty module was installed, the ARM Cortex-M33 terminal displays the following information:

Get Messgae From Master Side : "hello world!" [len : 12]

The user can then input an arbitrary string to the virtual RPMsg tty using the following echo command on Cortex-A terminal:

echo test > /dev/ttyRPMSG<num>
<num> here is the allocated ttyRPMsg channel number. Please find out the number in the file system by "ls" command.
Log below shows the output of the RPMsg-Lite str echo demo in the terminal window:

On the M33 terminal, the received string content and its length is output, as shown in the log.

Get Message From Master Side : "test" [len : 4]
Get New Line From Master Side