Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
USART EDMA example
Send back received data
Echo every 8 characters
When you input 8 characters, system will echo it by LPUART and them would be seen on the OpenSDA terminal.