Hardware rework

Debug console serial rework:

For details, refer Hardware Rework Guide for MIMXRT595-EVK and Murata M.2 Module.

Host wake-up controller pin rework:

Connect M.2 (pin 42) to JP26 (pin 4) with a wire.

Controller wake-up host pin rework:

  1. Remove resistors R709 on MIMXRT595-EVK.

  2. Solder 10K ohm resistor on the Murata 1XK M.2 Module at the location shown in the following figure.

Parent topic:Hardware Rework Guide for Low Power Feature on MIMXRT595-EVK and Murata 1XK M.2 Module