Start/Stop button

The “Start” button for the UI element appears in the idle state when the manufacturing process has either stopped or has not yet begun. To begin the manufacturing process, press the “Start” button. After pressing the “Start” button, the text on the button changes to “Stop” and acts like a stop button. Press the “Stop” button after the manufacturing process is complete or at any time to stop the process. Use the “Stop” button carefully to not stop while the command is being executed. Otherwise, an incomplete update may result in an unresponsive device.

Exit button

Press the “Exit” button to close the MfgTool application. The “Exit” button can only work in the idle state or when the “Start” button is active. The “Exit” button does not work when the device manufacturing is in progress. An error message dialog appears if the “Exit” button is pressed while manufacturing. Press the “Stop” button first to stop the manufacturing process, which activates the “Start” button. Then use the “Exit” button to close the window and shut down the MfgTool application.

Parent topic:Start/Stop button

Parent topic:GUI elements