BD file for i.MX RT bootable image generation
The BD file for i.MX RT bootable image generation usually consists of four blocks. These blocks are options, sources, constants, and section.
Options block
The following table shows the options used to generate a bootable image for the Options block.
Supported options in the “Options” block
Options |
Description |
|---|---|
Flags |
Generates unsigned, signed, encrypted boot images, and plugin images: |
startAddress |
Provides the starting address of the target memory where image should be loaded by ROM. |
ivtOffset |
Provides offset where the IVT data structure must appear in the boot image. The default is 0x400 if not specified.The valid value is 0x400 or 0x1000 for i.MX RT boot image. |
initialLoadSize |
Defines the start of the executable image data from elf or the srec file. The default value is 0x2000 if not specified.In general, this value should be 0x1000 or 0x2000. |
DCDFilePath |
Defines the path to DCD file.If not specified, the DCD pointer in the IVT will be set to NULL (0) else the dcd file contents will be loaded at offset 0x40 from ivtOffset. The dcd file size is limited to (initialLoadSize - ivtOffset-0x40). |
cstFolderPath |
Defines the path for platform dependent CST. (windows, linux)If not specified, elftosb tool will search for cst executable in same path as elftosb executable. |
entryPointAddress |
Provides the entry point address for ELF or SREC image.If not specified, ELF image uses its source image entry point address but SREC image will use default entry point address (0). |
Parent topic:BD file for i.MX RT bootable image generation
Sources block
Typically, all the application image paths are provided in this section. Currently, the ELF file and SREC file are supported for i.MX RT Bootable image generation, for example:
sources {
elfFile = extern(0);
}
Parent topic:BD file for i.MX RT bootable image generation
Constants block
The Constants block provides a constant variable that is used to generate CSF data for image authentication and decryption. The Constants block is optional for an unsigned image. The supported constants are listed below.
Constants {
SEC_CSF_HEADER = 20;
SEC_CSF_INSTALL_SRK = 21;
SEC_CSF_INSTALL_CSFK = 22;
SEC_CSF_INSTALL_NOCAK = 23;
SEC_CSF_AUTHENTICATE_CSF = 24;
SEC_CSF_INSTALL_KEY = 25;
SEC_CSF_ AUTHENTICATE_DATA = 26;
SEC_CSF_INSTALL_SECRET_KEY = 27;
SEC_CSF_DECRYPT_DATA = 28;
SEC_NOP = 29;
SEC_SET_MID = 30;
SEC_SET_ENGINE = 31;
SEC_INIT = 32;
SEC_UNLOCK = 33;
}
Parent topic:BD file for i.MX RT bootable image generation
Section blocks
The Section blocks are used to create the sections for an i.MX RT bootable image, for example, all sections for CSF data. For the unsigned image, the Section block is a fixed blank section, as shown below.
section (0)
{
}
For signed and encrypted image, the following sections are defined for the elftosb utility to generate the CSF descriptor file which is required by CST for CSF data generation.
SEC_CSF_HEADER
This section defines the necessary elements required for CSF Header generation as well as default values used for other sections throughout the remaining CSF.
Elements for CSF Header section generation
Element |
Description |
|---|---|
Header_Version |
HAB library version |
Header_HashAlgorithm |
Default Hash Algorithm |
Header_Engine |
Default Engine |
Header_EngineConfiguration |
Default Engine Configuration |
Header_CertificateFormat |
Default Certificate Format |
Header_SignatureFormat |
Default signature format |
Header_SecurityConfiguration |
Fused security configuration |
Header_UID |
Generic (matches any value) |
Header_CustomerCode |
Value expected in “customer code” fuses |
An example section block is shown as follows.
section (SEC_CSF_HEADER;
Header_Version="4.3",
Header_HashAlgorithm="sha256",
Header_Engine="DCP",
Header_EngineConfiguration=0,
Header_CertificateFormat="x509",
Header_SignatureFormat="CMS"
)
{
}
SEC_CSF_INSTALL_SRK
This section contains the elements to authenticate and install the root public key for use in subsequent sections, as shown in the following table.
Elements for CSF Install SRK section generation
Element |
Description |
|---|---|
InstallSRK_Table |
Path pointing to the Super Root Key Table file |
InstallSRK_Source |
SRK index with the SRK table |
InstallSRK_HashAlgorithm |
SRK table hash algorithm. |
An example section block is shown as follows.
section (SEC_CSF_INSTALL_SRK;
InstallSRK_Table="keys/SRK_1_2_3_4_table.bin", // "valid file path"
InstallSRK_SourceIndex=0
)
{
}
SEC_CSF_INSTALL_CSFK
This section consists of the elements used to authenticate and install a public key for use in subsequent sections.
Elements for CSF Install CSFK section generation
Element |
Description |
|---|---|
InstallCSFK_File |
File path pointing to CSFK certificate |
InstallCSFK_CertificateFormat |
CSFK certificate format |
section (SEC_CSF_INSTALL_CSFK;
InstallCSFK_File="crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem", // "valid file path"
InstallCSFK_CertificateFormat="x509" // "x509"
)
{
}
SEC_CSF_INSTALL_NOCAK
The Install NOCAK command authenticates and installs a public key for use with the fast authentication mechanism (HAB 4.1.2 and up). With this mechanism, one key is used for all signatures.
The following table lists the install NOCAK command arguments.
Elements for CSF Install NOCAK section generation
Element |
Description |
|---|---|
InstallNOCAK_File |
File path pointing to CSFK certificate |
InstallNOCAK_CertificateFormat |
CSFK certificate format |
An example section block is shown as follows:
section (SEC_CSF_INSTALL_NOCAK;
InstallNOCAK_File= "crts/SRK1_sha256_2048_65537_v3_usr_crt.pem") // "valid file path"
InstallNOCAK_CertificateFormat= "WTLS" // "WTLS", "X509"
)
{
}
SEC_CSF_AUTHENTICATE_CSF
This section is used to authenticate the CSF from which it is executed using the CSFK mentioned in the section above. See the following table for more details.
Elements for CSF Authenticate CSF section generation
Element |
Description |
|---|---|
AuthenticateCSF_Engine |
CSF signature hash engine |
AuthenticateCSF_EngineConfiguration |
Configuration flags for the hash engine. Note that the hash is computed over an internal RAM copy of the CSF |
AuthenticateCSF_SignatureFormat |
CSF signature format |
An example section block is shown as follows:
section (SEC_CSF_AUTHENTICATE_CSF)
{
}
SEC_CSF_INSTALL_KEY
This section consists of elements used to authenticate and install a public key for use in subsequent sections, as shown in the following table.
Elements for CSF Install Key section generation
Element |
Description |
|---|---|
InstallKey_File |
File path pointing to a Public key file |
InstallKey_VerificationIndex |
Verification key index in Key store |
InstallKey_TargetIndex |
Target key index in key store |
InstallKey_CertificateFormat |
Valid values: WTLS, X509 |
InstallKey_HashAlgorithm |
Hash algorithm for certificate binding. |
section (SEC_CSF_INSTALL_KEY;
InstallKey_File="crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem",
InstallKey_VerificationIndex=0, // Accepts integer or string
InstallKey_TargetIndex=2) // Accepts integer or string
{
}
SEC_CSF_AUTHENTICATE_DATA
This section contains elements that are used to verify the authenticity of pre-loaded data in memory.
Elements for CSF Authenticate Data section generation
Element |
Description |
|---|---|
AuthenticateData_VerificationIndex |
Verification key index in key store |
AuthenticateData_Engine |
Data signature hash engine |
AuthenticateData_EngineConfiguration |
Configuration flags for the engine |
AuthenticateData_SignatureFormat |
Data signature format |
AuthenticateData_Binding |
64-bit unique ID (UID) for binding. |
An example section block is shown as follows:
section (SEC_CSF_AUTHENTICATE_DATA;
AuthenticateData_VerificationIndex=2,
AuthenticateData_Engine="DCP",
AuthenticateData_EngineConfiguration=0)
{
}
SEC_CSF_INSTALL_SECRET_KEY
This section contains elements used to install the secret key to the MCU secret key store which is used for KeyBlob decryption. This section is required for encrypted image generation and not for signed image.
Elements for CSF Install Secret Key section generation
Element |
Description |
|---|---|
SecretKey_Name |
Specifies the file path used for CST to generate the random decryption key file |
SecretKey_Length |
Key length in bits |
SecretKey_VerifyIndex |
Master KEK index |
SecretKey_TargetIndex |
Target secret key store index |
SecretKey_BlobAddress |
Internal or external DDR address |
An example section block is shown as follows:
section (SEC_CSF_INSTALL_SECRET_KEY;
SecretKey_Name="dek.bin",
SecretKey_Length=128,
SecretKey_VerifyIndex=0,
SecretKey_TargetIndex=0)
{
}
SEC_CSF_DECRYPT_DATA
This section is required for encrypted image generation and not for signed image. It contains the necessary elements used to decrypt and authenticate a list of code/data blocks using the secret key stored in the secret key store, as shown in the following table.
Elements for CSF Decrypt Data section generation
Element |
Description |
|---|---|
Decrypt_Engine |
MAC engine |
Decrypt_EngineConfiguration |
Configuration flags for the engine |
Decrypt_VerifyIndex |
Secret key index in the Secret key store |
Decrypt_MacBytes |
Size of MAC in bytes |
An example section block is shown as follows.
section (SEC_CSF_DECRYPT_DATA;
Decrypt_Engine="DCP",
Decrypt_EngineConfiguration="0", // "valid engine configuration values"
Decrypt_VerifyIndex=0,
Decrypt_MacBytes=16)
{
}
SEC_NOP
The command in this section has no effect. It also has no arguments.
An example section block is shown as follows.
section (SEC_NOP)
// NOP command has no arguments
{
}
SEC_SET_MID
The Set MID command selects a range of fuse locations to use as a manufacturing identifier (MID). MID values are bound with Authenticate Data signatures when verified using keys with the MID binding flag in the Install Key command.
Elements for CSF Set MID section generation
Element |
Description |
|---|---|
SetMID_Bank |
Fuse bank containing MID. |
SetMID_Row |
Starting row number of MID within bank. |
SetMID_Fuse |
Starting fuse of MID within row. |
SetMID_Bits |
Number of bits for MID. |
An example section block is shown as follows:
section (SEC_SET_MID;
SetMID_Bank = 4,
SetMID_Row = 0,
SetMID_Fuse = 7,
SetMID_Bits = 64)
{
}
SEC_SET_ENGINE
The Set Engine command selects the default engine and engine configuration for a given algorithm.
Elements for CSF Set Engine section generation
Element |
Description |
|---|---|
SetEngine_Engine |
Engine |
SetEngine_HashAlgorithm |
Hash algorithm |
SetEngine_EngineConfiguration |
Configuration flags for the engine. |
An example section block is shown as follows:
section (SEC_SET_ENGINE;
SetEngine_HashAlgorithm = "sha256",
SetEngine_Engine = "DCP",
SetEngine_EngineConfiguration = "0")
{
}
• SEC_INIT
The Init command initializes specified engine features when exiting the internal BootROM.
Elements for CSF Init section generation
Element |
Description |
|---|---|
INIT_Engine |
Engine to initialize |
INIT_Features |
Comma-separated list of features to initialize |
An example section block is shown as follows:
section (SEC_INIT;
Init_Engine = "SRTC")
// Init_Features= "MID"
{
}
• SEC_UNLOCK
The Unlock command prevents specified engine features from being locked when exiting the internal BootROM.
Elements for CSF Unlock section generation
Element |
Description |
|---|---|
Unlock_Engine |
Engine to unlock |
Unlock_features |
Comma-separated list of features to unlock |
Unlock_UID |
Device specific 64-bit UID |
An example section block is shown as follows:
section (SEC_UNLOCK;
Unlock_Engine = "OCOTP",
Unlock_features = "JTAG, SRK REVOKE",
Unlock_UID = "0x01, 0x23, 0x45, 0x67, 0x89, 0xab, 0xcd, 0xef")
{
}
Parent topic:BD file for i.MX RT bootable image generation
Parent topic:Description of the elftosb utility