Functions

The following Analogue Output (Basic) cluster function is provided in the NXP implementation of the ZCL:

The cluster attributes can be accessed using the general attribute read/write functions, as described in Section 2.3.

eCLD_AnalogOutputBasicCreateAnalogOutputBasic

teZCL_Status eCLD_AnalogOutputBasicCreateAnalogOutputBasic(
    tsZCL_ClusterInstance *psClusterInstance,
    bool_t bIsServer,
    tsZCL_ClusterDefinition *psClusterDefinition,
    void *pvEndPointSharedStructPtr,
    uint8 *pu8AttributeControlBits);    

Description

This function creates an instance of the Analogue Output (Basic) cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.

The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function will create an Analogue Output (Basic) cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.

Note: This function must not be called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.

When used, this function must be called after the stack has been started and after the ZCL has been initialized.

The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the Analog Output Basic cluster.

The function initializes the array elements to zero.

Parameters

  • psClusterInstance        Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.

  • bIsServer         Type of cluster instance (server or client) to be created:

  • TRUE - server

  • FALSE - client

  • psClusterDefinition        Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Analogue Output (Basic) cluster. This parameter can refer to a pre-filled structure called sCLD_AnalogOutputBasic which is provided in the AnalogOutputBasic.h file.

  • pvEndPointSharedStructPtr        Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type tsCLD_AnalogOutputBasic which defines the attributes of Analogue Output (Basic) cluster. The function initializes the attributes with default values.

  • pu8AttributeControlBits        Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_INVALID_VALUE

Parent topic:Functions

Parent topic:Analogue Output (Basic)