eCLD_ColourControlCommandColourLoopSetCommandSend

teZCL_Status eCLD_ColourControlCommandColourLoopSetCommandSend(
        uint8 u8SourceEndPointId,
        uint8 u8DestinationEndPointId,
        tsZCL_Address *psDestinationAddress,
        uint8 *pu8TransactionSequenceNumber,
        tsCLD_ColourControl_ColourLoopSetCommandPayload
    *psPayload);

Description

This function sends a Colour Loop Set command to instruct a device to configure the movement of the ‘enhanced current hue’ attribute value around the colour loop corresponding to the CIE colour ‘triangle’. The configured movement can be started in either direction and for a specific duration. The start hue, direction and duration are specified in the payload of the command (see Section 31.7.2). The ‘current hue’ attribute is also moved through values based on the ‘enhanced current hue’ value.

The function can also be used to stop existing movement around the colour loop.

The device receiving this message will generate a callback event on the endpoint on which the Colour Control cluster was registered. The device must first ensure that ‘hue and saturation’ mode is selected by setting the ‘colour mode’ attribute to 0x00 and that ‘enhanced hue and saturation’ mode is selected by setting the ‘enhanced colour mode’ attribute to 0x03, if required. It can then move the ‘enhanced current hue’ value as requested.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

This function can only be used when the ‘enhanced current hue’ attribute is enabled in the Colour Control cluster.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent

  • psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

  • *psPayload: Pointer to a structure containing the payload for this message (see Section 31.7.2)

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions