eCLD_ColourControlCommandEnhancedMoveToHueCommandSend
teZCL_Status eCLD_ColourControlCommandEnhancedMoveToHueCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ColourControl_EnhancedMoveToHueCommandPayload
*psPayload);
Description
This function sends an Enhanced Move to Hue command to instruct a device to move its ‘enhanced current hue’ attribute to a target hue value in a continuous manner within a given time. The enhanced hue value, direction and transition time are specified in the payload of the command (see Section 31.7.2). The ‘current hue’ attribute is also moved to a value based on the target ‘enhanced current hue’ value.
Since the possible hues are represented on a closed boundary, the target hue can be reached by moving the attribute value in either direction, up or down (the attribute value wraps around). Options are also provided for ‘shortest route’ and ‘longest route’ around the boundary.
The device receiving this message will generate a callback event on the endpoint on which the Colour Control cluster was registered. The device must first ensure that ‘hue and saturation’ mode is selected by setting the ‘colour mode’ attribute to 0x00 and that ‘enhanced hue and saturation’ mode is selected by setting the ‘enhanced colour mode’ attribute to 0x03, if required. It can then move the ‘enhanced current hue’ value as requested.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
This function can only be used when the ‘enhanced current hue’ attribute is enabled in the Colour Control cluster.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload: Pointer to a structure containing the payload for this message (see Section 31.7.2)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions