eCLD_ColourControlCommandMoveSaturationCommandSend

teZCL_Status eCLD_ColourControlCommandMoveSaturationCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ColourControl_MoveSaturationCommandPayload
*psPayload);

Description

This function sends a Move Saturation command to instruct a device to move its ‘current saturation’ attribute value in a given direction at a specified rate for an indefinite time. The direction and rate are specified in the payload of the command (see Section 31.7.2).

The command can request that the saturation is moved up or down, or that existing movement is stopped. Once started, the movement will continue until it is stopped. If the current saturation reaches its minimum or maximum value, the movement will automatically stop.

The device receiving this message will generate a callback event on the endpoint on which the Colour Control cluster was registered. The device must first ensure that ‘hue and saturation’ mode is selected by setting the ‘colour mode’ attribute to 0x00, if required. It can then move the ‘current saturation’ value as requested.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

This function can only be used when the ‘current saturation’ attribute is enabled in the Colour Control cluster.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent

  • psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

  • *psPayload: Pointer to a structure containing the payload for this message (see Section 31.7.2)

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions