eCLD_ColourControlCommandStepColourTemperatureCommandSend
teZCL_Status eCLD_ColourControlCommandStepColourTemperatureCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ColourControl_StepColourTemperatureCommandPayload
*psPayload);
Description
This function sends a Step Colour Temperature command to instruct a device to increase or decrease its ‘mired colour temperature’ attribute by a specified ‘step’ value in a continuous manner within a given time. The attribute value is a scaled reciprocal of colour temperature, as indicated in Section 31.5.4. The step size, direction and transition time are specified in the payload of the command (see Section 31.7.2). Maximum and minimum attribute values for the movement are also specified in the payload.
The command can request that the attribute value is moved up or down. If this value reaches the specified maximum or minimum before the required change has been achieved, the movement will automatically stop.
The movement through colour space will follow the ‘Black Body Line’.
The device receiving this message will generate a callback event on the endpoint on which the Colour Control cluster was registered. The device must first ensure that ‘colour temperature’ mode is selected by setting the ‘colour mode’ attribute to 0x02, if required. It can then move the ‘mired colour temperature’ value as requested.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
This function can only be used when the ‘mired colour temperature’ attribute is enabled in the Colour Control cluster, as well as the ‘mired colour temperature maximum’ and ‘mired colour temperature minimum’ attributes.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
*psPayload: Pointer to a structure containing the payload for this message (see Section 31.7.2)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions