eCLD_IASACE_BypassSend

teZCL_Status eCLD_IASACE_BypassSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_IASACE_BypassPayload *psPayload); 

Description

This function can be used on an IAS ACE cluster client to send an IAS ACE Bypass command to an IAS ACE server. This command instructs the server to take one or more specified zones out of the system for the current activation.

Note: The bypassed zones will be reinstated the next time the system is disarmed. To exclude them again the next time the system is armed, the Bypass command must be re-sent before sending the Arm command.

The outcome of the request will be returned by the server in a response which will generate an E_CLD_IASACE_CMD_BYPASS_RESP event when received on the client.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the command and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

  • psPayload: Pointer to a structure containing the payload for the command (see Section 38.7.5)

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions