eCLD_LevelControlCommandMoveCommandSend
teZCL_Status eCLD_LevelControlCommandMoveCommandSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
bool_t bWithOnOff,
tsCLD_LevelControl_MoveCommandPayload
*psPayload);
Description
This function sends a Move command to instruct a device to move its ‘current level’ attribute either up or down in a continuous manner at a specified rate. The direction and rate are specified in the payload of the command (see Section 16.8.3).
If the current level reaches the maximum or minimum permissible level for the device, the level change stops.
The device receiving this message generates a callback event on the endpoint on which the Level Control cluster is registered, and move the current level in the direction and at the rate specified.
The option is provided to use this command in association with the On/Off cluster. In this case:
If the command is to increase the current level, the OnOff attribute of the On/Off cluster is set to ‘on’.
If the command decreases the current level to the minimum permissible level for the device, the OnOff attribute of the On/Off cluster is set to ‘off’.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
bWithOnOff: Specifies whether this cluster interacts with the On/Off cluster:
TRUE - interaction
FALSE - no interaction
psPayload: Pointer to a structure containing the payload for this message (see Section 16.8.3)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions